Eaton Logo

Is a neutral sensor required for breakers with ground fault?

If there are no neutral loads the neutral sensor is not necessary.  If the system neutral is grounded, but no phase to neutral loads are used, the neutral current sensor is not necessary. In that case, the white and grey leads on the trip unit should be capped or taped.