Eaton Logo

Are there any additional Ground / Neutral Lugs for BR Loadcenter?

On the BR load centers, if an additional ground / neutral lug is needed, then select from the following:

 

NL20   -- Wire Size #2/0 Maximum

NL30   -- Wire Size #3/0 Maximum

NL300 -- Wire Size 300 KCMIL Maximum