Eaton Logo

Looking for a manual transfer switch.

The description manual transfer switch can be used to identify several different types of products.

It could be as simple as a double throw safety switch which are listed in the Volume 2, Tab 01 section of the catalog under Double Throw Switches

If a UL listed Manual Transfer Switch is needed the Commercial Transfer Switch group should be able to assist by phone at 877-386-2273 option 2, option 4, option 3. 

There is also a manual transfer switch available in the rotary disconnect switch product offering.  These are listed in the Volume 5, Tab08 as Manual Transfer/Double Throw Switches