Eaton Logo

I'm looking for a DC safety switch

Eaton offers a few different options for DC voltage on safety switches.

1.  The standard switches can be used for DC voltages when the poles are wired in series in the field.  See catalog or individual switch publication for details.

2.  There are DC rated switches that have the poles wired in series from the factory with bus bars.  See following link for DC Disconnects for Solar Photovoltaic Installation

3.  There are also DC switches that use permanent magnets to allow 600VDC to be handled by a single pole of the switch.  See following link for DC Disconnects for Grounded and Ungrounded Photovoltaic Installation