What are the wire sizes that a BAB breaker will accept?
The wire sizing and corresponding Torque values are embossed on the side of the breaker itself as following:
14-10 AWG 20 in-lbs
8 AWG 25 in-lbs
6-4 AWG 27 in-lbs
3-1/0 AWG 45 in-lbs
Thus, the range for wires is 14 to 1/0.