Eaton Logo

Advantage Programming Module (WAPM)

The advantage programming module is used to omit the factory standard  advance protective features of the Advantage W200 starters. You can omit the Ground fault, Phase Lost and  Phase Unbalance protection with the WAPM.  the WAPM will not turn off overload protection. 

How do I replace Advantage Starters with Freedom AN19 starters in UL 508A Applications?

What is the replacement board for installed Advantage Starters?