How do I wire multiple start/stop pushbutton stations to a motor starter?
See attached wiring schematic below (scroll down) for wiring more than one momentary start/stop pushbutton station to a typical motor starter that has a Normally Open auxiliary contact on it, which is required.
For a more detailed explanation or other wiring variations, please contact the TRC at 1-800-ETN-CARE and hit the option for technical support then contactors/starters.