MMX (M-Max) How to Default and Program Drive
M-Max (MMX) Quick-Start Guide:
Introduction:
This guide sets up an M-Max (MMX) to be able to run a variety of configurations. For this guide default the drive to clear all parameter changes. Make sure to have motor name plate information on hand. You will need:
- Motor Nominal Voltage
- Motor Nominal (FLA) Rated Current
- Motor Nominal Frequency
- Motor Nominal RPM
- Motor Power Factor (P.F.)
- Motor Service Factor (S.F.)
Navigating the Menu and Changing Parameters:
The MMX menu navigation is unique and requires timing to change parameter values. The figure below shows the keypad screen. The next page shows the keypad interface and what the indicators represent.
Figure 1: MMX Keypad P1.1
Arrow Indicators:
- READY: Indicates that DC-Bus and Enable Signals are present; drive can run
- RUN: Indicates if the drive is running, does NOT mean motor has to be rotating
- STOP: Drive is stopped and the motor is not being powered
- ALARM: Indicates if there is an issue that may be arising, i.e. Current Limit
- FAULT: Indicates that the drive has a fault condition present, i.e. Ext Fault
- REF: Indicates the keypad Reference value, use for keypad speed ref. only
- MON: Indicates Monitor menu, use to monitor Output Freq, Voltages, Inputs, etc.
- PAR: Indicates Parameter menu, use to change any parameter and drive setting
- FLT: Indicates Fault Menu, use to see drive status at time fault occurred
- FWD: Indicates if drive is running in forward direction
- REV: Indicates if drive is running in reverse direction
- I/O: Indicates if drive is under I/O Terminal (Remote) Control for START/STOP signals
- KEYPAD: Indicates if drive is under Keypad (Local) Control for START/STOP signals
- BUS: Indicates if drive is under Fieldbus Control for START/STOP signals
Changing a Parameter Value:
Changing a parameter value in a MMX requires the user to wait until the value is displayed on screen. The example below shows how to change the value for P1.1.
Note: The MMX will always alternate between showing the Parameter location and the Parameter value. Changing values requires timing of the button presses. |
Example: How to Change a Parameter on the MMX
Step 1: Changing from MON menu to PAR menu. Press the BACK/RESET button
Figure 2: Monitor (MON) Menu
Step 2: The screen will become blank except for the indicator arrows.
Figure 3: Menu Selection – MON Selected
Step 3: Use the ▼(down) arrows to change to the Parameter Menu (PAR).
Figure 4: Menu Selection - PAR selected
Step 4: Press OK button to select the Parameter Menu
Figure 5: Menu Location P1.1
Step 5: Wait till P1.1 value is displayed, the value will show “1” by default. Press OK button.
Step 6: Use the ▼(down) arrow to change to “0” value,
Figure 6: P1.1 Initial Value = 1
Step 7: Press the OK button to save the parameter value. Once saved, the “0” will stop, blinking. The display will resume showing the P1.1 and new value “0” in the original alternating fashion.
Step 8: Changing the parameter is complete
Defaulting the Drive:
Defaulting an MMX can be done by following the steps below. This process will clear any changes made to the drive. Motor nameplate values will be needed to reprogram the drive.
Step 1: Navigate to P1.1
Figure 7: Menu Location P1.1
Step 2: Use ▼(down) arrow to find parameter S4.2
Figure 8: Menu Location S4.2
Step 3: S4.2 is by default “0.” Change this parameter to “1.” After changing to “1” then press the OK button. The drive will then power cycle. You will also need to change P1.1 back to “0” to have access to all parameter groups again. The drive will automatically change S4.2 back to 0 after power cycling. No need to change back.
Analog Inputs:
The MMX drive has 2 analog inputs, by default AI1 is 0-10VDC and AI2 is 4-20mA input. See the figure below for wiring to the inputs.
- AI1 uses PIN1 (VCC), PIN2 (Potentiometer Variable Output) and PIN3 (GND)
- AI2 uses PIN4 (Signal Plus [+]) and PIN5 (Signal Negative [-])
Programming the Drive:
Default the drive by going to parameters and set S4.2 to “1”. Next set P1.1 to “0”. Next select the application at P1.2 to match your motor load/application. Continue to set the following parameters found in the table below. Once all the parameters in the table are completed, choose the correct yellow highlighted sections on the following pages to complete programming the drive. Follow the steps exactly.
Standard Parameters Table:
Choose Application Mode Based on site application. If you cannot determine which application mode fits best, use BASIC [0]. Set parameters to value in respective column. This must be done for any Control Scheme |
Table 1: Standard Parameter Table Settings
Parameter |
Designation |
Basic [0] |
Pump [1] |
Fan [2] |
High Load [3] |
P1.1 |
Quick Start Parameters |
0 |
0 |
0 |
0 |
P1.2 |
Application |
0 |
1 |
2 |
3 |
P6.3 |
Minimum Frequency [Hz] |
00.00Hz |
20.00Hz |
20.00Hz |
00.00Hz |
P6.4 |
Maximum Frequency [Hz] |
60.00Hz |
60.00Hz |
60.00Hz |
60.00Hz |
P6.5 |
Accel. Time 1 [sec] |
10.0s |
15.0s |
20.0s |
5.0s |
P6.6 |
Decel. Time 1 [sec] |
10.0s |
15.0s |
20.0s |
5.0s |
P6.7 |
Start Function |
0/Ramp |
0/Ramp |
0/Ramp |
0/Ramp |
P6.8 |
Stop Function |
0/Coast |
1/Ramp |
0/Coast |
0/Coast |
P7.1 |
Motor Rated Current [Amps] |
NP |
NP |
NP |
NP |
P7.2 |
Current Limit [Amps] |
** |
** |
** |
** |
P7.3 |
Motor Rated Speed [RPM] |
NP |
NP |
NP |
NP |
P7.4 |
Motor Power Factor [0 ≤ P.F. ≤1] |
NP |
NP |
NP |
NP |
P7.5 |
Motor Voltage [VRMS] |
NP |
NP |
NP |
NP |
P7.6 |
Motor Rated Freq. [Hz] |
NP |
NP |
NP |
NP |
NP: Name plate values on the Motor
**
Where Service Factor is 1 ≤ S.F. ≤ 1.5 (always between 1.0 and 1.5)
If the methods below do not fit the desired control or if there are any issues. Please call the TRC at 1-800-322-4986 Opt 4. Available Monday through Friday 08:00-17:00 (CST). |
Start/Stop by Keypad and Speed Reference from Keypad:
The following parameters must be changed after completing the Standard Parameters table
- P6.2 Primary Remote Speed Reference = 1
- Set the Drive to KEYPAD control by pressing the LOC/REM button, check the arrow indicator.
- Drive will start/stop by keypad buttons alone. Once started, screen will change from PAR menu to REF menu.
- Initially, the REF speed will the minimum frequency value (P6.3). If that is zero, then so will the Keypad Reference.
- At the REF menu change the frequency with the ▲(Up) Arrow and the ▼(Down) Arrow [Might need to press OK button to be able to change value].
- Use the ►(Right) Arrow to be able to select the digits. Then you can use ◄(Left) Arrow and ►(Right) Arrow to change digit selection.
Start/Stop by Keypad and Speed Reference from AI1/AI2:
The following parameters must be changed after completing the Standard Parameters table
- P6.2 Primary Remote Speed Reference = 3 (AI1 [0-10V]) or 4 (AI2 [4-20mA])
- P6.1 Primary Remote Control Source = 2
- Set the Drive to KEYPAD control by pressing the LOC/REM button, check the arrow indicator.
- Drive will start/stop by keypad buttons alone. Once started, the drive will use the AI1 or AI2 as the speed reference.
Note: See Analog Inputs, pg. 7 for wiring and selection of analog inputs |
Start/Stop I/O Terminal and Speed Reference from Keypad:
The following parameters must be changed after completing the Standard Parameters table
- P6.2 Primary Remote Speed Reference = 1
- Set Drive to I/O control by pressing the LOC/REM button, check the arrow indicator.
- Drive will start/stop by the I/O Terminal, DI1 (PIN 8) will need to have 24VDC applied. Once started, screen will change from PAR menu to REF menu.
- Initially, the REF speed will the minimum frequency value (P6.3). If that is zero, then so will the Keypad Reference.
- At the REF menu change the frequency with the ▲(Up) Arrow and the ▼(Down) Arrow [Might need to press OK button to be able to change value].
- Use the ►(Right) Arrow to be able to select the digits. Then you can use ◄(Left) Arrow and ►(Right) Arrow to change digit selection
Start/Stop by I/O Terminal and Speed Reference from AI1/AI2:
The following parameters must be changed after completing the Standard Parameters table
- P6.2 Primary Remote Speed Reference = 3 (AI1) or 4 (AI2)
- Set Drive to I/O control by pressing the LOC/REM button, check the arrow indicator.
- Drive will start/stop by the I/O Terminal, DI1 (PIN 8) will need to have 24VDC applied.
- Drive will follow the reference provided by AI1 or AI2 (Select with P6.2)
Note: See Analog Inputs, pg. 7 for wiring and selection of analog inputs |
Start/Stop by I/O Terminal and Speed Reference from Fixed Frequency:
The following parameters must be changed after completing the Standard Parameters table
- P6.2 Primary Remote Speed Reference = 0
- P10.1 Fixed Frequency FF0 = USER DESIRED FREQ. [Hz]
- Set Drive to I/O control by pressing the LOC/REM button, check the arrow indicator.
- Drive will start/stop by the I/O Terminal, DI1 (PIN 8) will need to have 24VDC applied.
PID Control – Keypad Setpoint – AI1/AI2 Transducer Reference:
Note: Drive will run motor when transducer signal is below setpoint |
The following parameters must be changed after completing the Standard Parameters table
- P9.1 PID Controller = 1 [Activated]
- P9.4 PID Controller Setpoint, keypad = Setpoint [%]
- P9.6 PID Controller Process Variable (Transducer Feedback) = 1 (AI1) or 2 (AI2)
- P9.9 PID Controller Inversion Control = 0 (Not Inverted)
- P9.12 Sleep Mode Frequency = USER DEFINED [Hz]
- This value CANNOT be the same as the P6.3 Minimum Frequency, needs to be different (i.e. min freq. = 20.00 Hz, Sleep Mode Freq = 20.01 Hz)
- P9.13 Sleep Mode Wake Up Point = USER DEFINED BELOW SETPOINT [%]
- P9.14 Sleep Mode Delay Time = USER DEFINED [sec]
- Set Drive to I/O control by pressing the LOC/REM button, check the arrow indicator.
- Drive will start/stop by the I/O Terminal, DI1 (PIN 8) will need to have 24VDC applied.
- Drive will run PID algorithm when start signal is applied. When output frequency drops below Sleep Mode Freq., the drive will stop running, until Wake-Up point is reached by going below Setpoint [%].
Note: See Analog Inputs, pg. 7 for wiring and selection of analog inputs |
Inverted PID Control – Keypad Setpoint – AI1/AI2 Transducer Reference:
Note: Drive will run motor when transducer signal is above setpoint |
The following parameters must be changed after completing the Standard Parameters table
- P9.1 PID Controller = 1 [Activated]
- P9.4 PID Controller Setpoint, keypad = Setpoint [%]
- P9.6 PID Controller Process Variable (Transducer Feedback) = 1 (AI1) or 2 (AI2)
- P9.9 PID Controller Inversion Control = 1 (Inverted)
- P9.12 Sleep Mode Frequency = USER DEFINED [Hz]
- This value CANNOT be the same as the P6.3 Minimum Frequency, needs to be different (i.e. min freq. = 20.00 Hz, Sleep Mode Freq = 20.01 Hz)
- P9.13 Sleep Mode Wake Up Point = USER DEFINED ABOVE SETPOINT [%]
- P9.14 Sleep Mode Delay Time = USER DEFINED [sec]
- Set Drive to I/O control by pressing the LOC/REM button, check the arrow indicator.
- Drive will start/stop by the I/O Terminal, DI1 (PIN 8) will need to have 24VDC applied.
- Drive will run PID algorithm when start signal is applied. When output frequency drops below Sleep Mode Freq., the drive will stop running, until Wake-Up point is reached by going above Setpoint [%].
Note: See Analog Inputs, pg. 7 for wiring and selection of analog inputs |
Auto-Start after Power Loss – AI1/AI2 Transducer Reference:
The following parameters must be changed after completing the Standard Parameters table
- P3.1 Start/Stop-Logic = 0
- P6.2 Primary Remote Speed Reference = 3 (AI1) or 4 (AI2)
- Set Drive to I/O control by pressing the LOC/REM button, check the arrow indicator.
- Drive will start/stop by the I/O Terminal, DI1 (PIN 8) will need to have 24VDC applied. This PIN can also be permanently jumpered 24VDC.
- Drive will follow the reference provided by AI1 or AI2 (Select with P6.2)
- If power is lost and then comes back, the drive will automatically restart, if start command is still present.
3-Wire Control (BAS-Start) – AI1/AI2 Transducer Reference:
The following parameters must be changed after completing the Standard Parameters table
- P3.1 Start/Stop-Logic = 2
- P6.2 Primary Remote Speed Reference = 3 (AI1) or 4 (AI2)
- Set Drive to I/O control by pressing the LOC/REM button, check the arrow indicator.
- Drive must have 24VDC (Normally Closed) on DIN2 (PIN 9), STOP Signal.
- Drive is looking for a momentary closure of DIN1 (PIN 8) with 24VDC, RUN Signal.
- Drive will follow the reference provided by AI1 or AI2 (Select with P6.2)
Additional Help
In the US or Canada please contact the LV Drives Technical Resource Center at 1-800-322-4986 or via email at TRCDrivesTechSupport@Eaton.com.
All other supporting documentation is located on the Eaton web site at www.eaton.com/drives.