M-Max (MMX) - Simple Setup Fan - Pump - Conveyor
Recommend to default the drive. This will ensure that no other parameters will conflict with the final configuration. Default the drive by going to parameters and set S4.2 to “1”. Next set P1.1 to “0”. Next select the application at P1.2 to match your motor load/application. Continue to set the following parameters found in the table below. Once all the parameters in the table are completed, choose the correct yellow highlighted sections on the following pages to complete programming the drive. Follow the steps exactly.
Standard Parameters Table:
Choose Application Mode Based on site application. If you cannot determine which application mode fits best, use BASIC [0]. Set parameters to value in respective column. This must be done for any Control Scheme |
Parameter |
Designation |
Basic [0] |
Pump [1] |
Fan [2] |
High Load [3] |
P1.1 |
Quick Start Parameters |
0 |
0 |
0 |
0 |
P1.2 |
Application |
0 |
1 |
2 |
3 |
P6.3 |
Minimum Frequency [Hz] |
00.00Hz |
20.00Hz |
20.00Hz |
00.00Hz |
P6.4 |
Maximum Frequency [Hz] |
60.00Hz |
60.00Hz |
60.00Hz |
60.00Hz |
P6.5 |
Accel. Time 1 [sec] |
10.0s |
15.0s |
20.0s |
5.0s |
P6.6 |
Decel. Time 1 [sec] |
10.0s |
15.0s |
20.0s |
5.0s |
P6.7 |
Start Function |
0/Ramp |
0/Ramp |
0/Ramp |
0/Ramp |
P6.8 |
Stop Function |
0/Coast |
1/Ramp |
0/Coast |
0/Coast |
P7.1 |
Motor Rated Current [Amps] |
NP |
NP |
NP |
NP |
P7.2 |
Current Limit [Amps] |
** |
** |
** |
** |
P7.3 |
Motor Rated Speed [RPM] |
NP |
NP |
NP |
NP |
P7.4 |
Motor Power Factor [0 ≤ P.F. ≤1] |
NP |
NP |
NP |
NP |
P7.5 |
Motor Voltage [VRMS] |
NP |
NP |
NP |
NP |
P7.6 |
Motor Rated Freq. [Hz] |
NP |
NP |
NP |
NP |
NP: Name plate values on the Motor
**
Where Service Factor is 1 ≤ S.F. ≤ 1.5 (always between 1.0 and 1.5)