M-Max (MMX) Start/Stop Keypad and Speed Reference by Keypad
Start/Stop by Keypad and Speed Reference from Keypad:
Begin programming the drive by entering the parameters in the table first. Then follow the steps below after that.
Parameter |
Designation |
Basic [0] |
Pump [1] |
Fan [2] |
High Load [3] |
P1.1 |
Quick Start Parameters |
0 |
0 |
0 |
0 |
P1.2 |
Application |
0 |
1 |
2 |
3 |
P6.3 |
Minimum Frequency [Hz] |
00.00Hz |
20.00Hz |
20.00Hz |
00.00Hz |
P6.4 |
Maximum Frequency [Hz] |
60.00Hz |
60.00Hz |
60.00Hz |
60.00Hz |
P6.5 |
Accel. Time 1 [sec] |
10.0s |
15.0s |
20.0s |
5.0s |
P6.6 |
Decel. Time 1 [sec] |
10.0s |
15.0s |
20.0s |
5.0s |
P6.7 |
Start Function |
0/Ramp |
0/Ramp |
0/Ramp |
0/Ramp |
P6.8 |
Stop Function |
0/Coast |
1/Ramp |
0/Coast |
0/Coast |
P7.1 |
Motor Rated Current [Amps] |
NP |
NP |
NP |
NP |
P7.2 |
Current Limit [Amps] |
** |
** |
** |
** |
P7.3 |
Motor Rated Speed [RPM] |
NP |
NP |
NP |
NP |
P7.4 |
Motor Power Factor [0 ≤ P.F. ≤1] |
NP |
NP |
NP |
NP |
P7.5 |
Motor Voltage [VRMS] |
NP |
NP |
NP |
NP |
P7.6 |
Motor Rated Freq. [Hz] |
NP |
NP |
NP |
NP |
The following parameters must be changed after completing the Standard Parameters table
- P6.2 Primary Remote Speed Reference = 1
- Set the Drive to KEYPAD control by pressing the LOC/REM button, check the arrow indicator.
- Drive will start/stop by keypad buttons alone. Once started, screen will change from PAR menu to REF menu.
- Initially, the REF speed will the minimum frequency value (P6.3). If that is zero, then so will the Keypad Reference.
- At the REF menu change the frequency with the ▲(Up) Arrow and the ▼(Down) Arrow [Might need to press OK button to be able to change value].
- Use the ►(Right) Arrow to be able to select the digits. Then you can use ◄(Left) Arrow and ►(Right) Arrow to change digit selection.