Eaton Logo

What does NRD mean on the PowerXL series drives keypad display

NRD means not ready.  Many times this is due to the run enable digital input not being read but it can also be a problem caused by the control module and power section not communicating.  Check the DC Link Voltage in the monitor menu.  If 0VDC, the power section is not communicating with the control module.  Unit temperature would also show as 0 C.  

Contact Tech Support (800-322-4986) for assistance to remedy this