Eaton Logo

Storage temperature for MCCB and MCP

Eaton MCP and MCCB product uses no material that would deteriorate under the long term effects of cold storage. Use -60 degrees C as a reasonable minimum storage temperature.  For maximum temperature, there are lubricants that could evaporate.  Maximum storage temperature should be +90 degrees C.  This recommended storage temperature of -60 to +90 degrees C is a conservative estimate.  If a wider range is needed, studies would need to be performed for verification.