Eaton Logo

How to select the Auxiliary contact material for the MCCB ?

Any load less than 150mA and less than 8VAC/DC should use gold plated or gold alloy contacts. for the voltages and currents above 150mA and  8VAC/DC, we recommend silver-flashed contacts for more robust and better suited for use.