Eaton Logo

How to: Select a replacement handle for a MDL breaker

The MDL uses the same replacement handle as the LD breaker. The handle can be mounted on MDL and HMDL breaker, however it cannot be mounted on sealed MDLB and HMDLB breakers.

Issue: Missing Trip Unit Mounting Screws for Series C, MDL Frame Breaker.

The trip unit mounting screws are assembled in the following manner; The outboard screws are assembled to the Frame, 2 for 2 pole, 2 for 3 pole, style 5113A57H08. The center screw is mounted in the Trip Unit, one 5113A57H09.