Eaton Logo

What are the mounting options for the Freedom contactors and starters?

The Freedom line of contactors and starters can be mounted in the horizontal or vertical position in the vertical plane. Line side should be on top or at the left when mounted. 

The springs and coils are designed to provide proper operation for the required mounting positions. Other methods of mounting due to effects of friction and gravity on the movement of the contactor parts creates mechanical stresses and can lead to failure.

Freedom Series Contactors and Starters Overview