Eaton Logo

Can an Eaton soft starter be connected Inside-the-Delta?

Yes. The S811+... soft starters can be configured to operate either in an inline or Inside-the-delta configuration. The Motor Wiring Config. parameter located in the Soft Start Config. Menu can be changed to enable the unit to operate in the Inside-the-Delta configuration.

NOTE: The Motor Nameplate FLA values will automatically shift when the Inside-the-Delta parameter option is selected.